2023-04-14 6:13 AM
Hi,
Looking for STM32 MCU in place of Microchip Controller ATSAM4S8BB-UUR.
Please suggest a suitable Controller.
2023-04-14 6:39 AM
120 MHz CM4 512KB FLASH 64-WLCSP
Nothing pin-for-pin / ball-for-ball
Should be some in the STM32L4(+) series with similar specs
The new STM32H5 might be worth a look. Also G0 or C0 depending on actual needs
Any specific features/function your current design uses? USART, I2C, counts, etc.
Floating Point Math?
RAM/FLASH utilization?
2023-04-14 7:15 AM
Low cost focus: STM32C0/STM32G0 (F0 upgrade)
Mainstream:general purpose STM32H5 (F4 upgrade)
Low power focus : STM32U5 (L4/L5 upgrade)
High Performance focus : STM32H7 (F7 upgrade)
There should be an STM32 Finder tool either on Android or PC to narrow down the choices depending on the memory footprint and specific peripherals. WLCSP is hardly for everyone. Form factor/high volume focus ?
2023-04-14 9:24 AM
Hi @KAjay.1,
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2023-04-16 11:17 PM
Hi,
Requirement is as below:
Core Processor - ARM® Cortex®-M4
Core Size - 32-Bit Single-Core,
Speed - 120MHz,
Program Memory Size -512KB (512K x 8),
Program Memory Type - FLASHRAM Size - 128K x 8,
Voltage - Supply (Vcc/Vdd) - 1.62V ~ 3.6V,
Data Converters - A/D 11x12b; D/A 2x12b,
Operating Temperature - -40°C ~ 85°C (TA)
Peripherals : UART - 1or2, I2C -2, SPI - 1or2, USB-1
2023-04-16 11:58 PM
These are just MCU parameters.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.