2022-01-18 9:11 AM
I'm looking for any examples that use the functions/methods/drivers found in the PDF: UM2298 User manual STM32Cube BSP drivers development guidelines .
I've installed the Board Support Package in my project and it specifically includes the files:
stm32l475e_iot01_env_sensors.c and .h
What I'm really looking for is an example that shows the proper usage of the
BSP_ENV_SENSOR_Enable() method. I've read the comments and to initialize the sensor I need to pass two args: Instance and Function. Both are uint32_t.
From the docs:
Instance 0 corresponds to HTS221 (temperature and humidity capabilities).
Instance 1 corresponds to LPS22HB (temperature and pressure capabilities).
#define ENV_SENSOR_INSTANCES_NBR 2U
#define ENV_SENSOR_FUNCTIONS_NBR 3U
#define ENV_TEMPERATURE 1U
#define ENV_PRESSURE 2U
#define ENV_HUMIDITY 4U
So If I want to init the HTS221 sensor for Temperature readings, the call would look like:
BSP_ENV_SENSOR_Enable(0, ENV_TEMPERATURE);
But this call returns the error code of -1
So I went looking for examples. I've tried every kind of search I can think of and all I get back are examples showing the older Board Support Package that uses different methods. I found the ST github repo for examples at:
https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/B-L475E-IOT01A/Examples/BSP
This was updated last month, so I figured it would be up to date. But it uses methods such as:
BSP_TSENSOR_ReadTemp();
This method is not in the PDF mentioned above.
So, anyone have any ideas?
Thanks,
Lance
2022-01-26 1:08 AM
Hello @LSmit.7 and welcome to the Community :)
I advise you to follow the step by step on wiki page Sensors usage with B-L475E-IOT01A, to configure and perform measurements with sensors available in the STM32L4 IoT Discovery kit.
Hope my answer helped you!
When your question is answered, please close this topic by choosing Select as Best.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.