2022-01-25 3:15 AM
2022-01-25 4:53 AM
Hello,
According to the datasheet there are no differences between stm32f103RC & stm32f103RE except the Flash size. I don't think this is related to the chip but may be to your hardware.
Is there a hardware difference between the two boards (PCB, crystal, CAN transceiver, etc ..)?
SofLit
2022-01-25 5:20 AM
Thanks for response.
Yes.They are in two different boards but I used other peripherals of STM32f103RC in my board.Only CAN bus doesn't work. I used external crystal 8MHz. CAN bus hasn't connected to other hardware. CANTX and CANRX is free. I observed CANTX on oscilloscope. It is High alltime. How do you think?
2022-01-25 5:36 AM
You haven't provided enough relevant information to diagnose the problem. There are many things that could be wrong, including hardware errors and software errors. Can you toggle the pin and observe on a scope? That is a starting point.
2022-01-25 8:15 PM
Yes.I toggle CANTX and CANRX pins and can observe on scope.
2022-01-26 12:33 AM
Hello,
We can't help you if you don't provide more details.
Could you please share the schematics of the boards at least CAN part (from GPIOs to CAN bus) and the crystal value of each board?
SofLit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.