2019-07-16 11:59 PM
Hi everyone,
I wonder how to know from which address start a program when we debug it into the flash memory and the finish address is easy to find if we know the start address.
according to the map of flash memory of the STM32F413 given by the link below:
On page 67: we see that there are some place which are reserved, I wonder if these place are reserved for the program through the ST-link?
or maybe if the program is more large then we will exceed these limits?
can someone cleared to me this point?
thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.