2019-07-17 2:38 AM
Cannot write to TIM3->EGR, Writes to EGR are stored in SR.
stm32g071xx.h definitions are correct.
Assembler output also shows correct addresses and offsets.
;;;1157 TIM3->DIER |= TIM_DIER_UIE;
0000b8 4608 MOV r0,r1
0000ba 68c0 LDR r0,[r0,#0xc]
0000bc 2101 MOVS r1,#1
0000be 4308 ORRS r0,r0,r1
0000c0 4922 LDR r1,|L20.332|
0000c2 60c8 STR r0,[r1,#0xc]
;;;1158 TIM3->SR |= TIM_SR_UIF;
0000c4 4608 MOV r0,r1
0000c6 6900 LDR r0,[r0,#0x10]
0000c8 2101 MOVS r1,#1
0000ca 4308 ORRS r0,r0,r1
0000cc 491f LDR r1,|L20.332|
0000ce 6108 STR r0,[r1,#0x10]
;;;1159 TIM3->EGR |= TIM_EGR_UG;
0000d0 4608 MOV r0,r1
0000d2 6940 LDR r0,[r0,#0x14]
0000d4 2101 MOVS r1,#1
0000d6 4308 ORRS r0,r0,r1
0000d8 491c LDR r1,|L20.332|
0000da 6148 STR r0,[r1,#0x14]
;;;1160 TIM3->CCMR1 |= TIM_CCMR1_CC1S;
0000dc 4608 MOV r0,r1
0000de 6980 LDR r0,[r0,#0x18]
0000e0 2103 MOVS r1,#3
0000e2 4308 ORRS r0,r0,r1
0000e4 4919 LDR r1,|L20.332|
0000e6 6188 STR r0,[r1,#0x18]
|L20.332|
DCD 0x40000400
But memory shows this.
Writes to DIER and CCMR1 are stored ok.
Writes to SR have no effect, nothing stored.
Writes to EGR are stored in SR.
0x40000400: 80 00 00 00 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00 03 00 00 00
// CR1 CR2 SMCR SR EGR CCMR1
Bug in STM32G071RB ?
Errata sheet has no matching issue...
Best regard
Juergen
2019-07-17 2:46 AM
TIM->EGR is write only. Writes 1 to some EGR register triggers some event. So how do you find out that writes to EGR do not succeed?
2019-07-17 2:52 AM
Aaah, thank you for making this clear and sorry for my misunderstanding.
The write to EGR.UG generates the event and as follow up SR.UIF shows that this event is now pending.
Best regards
Juergen
2019-07-17 3:19 AM
Wondering of SR.UIF set, as timer is still disabled.
So counter should not overflow.
My TIM3 setup is as this:
TIM3->ARR = (SystemCoreClock / CurrentSampleRate) - 1;
TIM3->CR1 |= TIM_CR1_ARPE; // ARR buffered
TIM3->EGR |= TIM_EGR_UG; // Force update generation (UG = 1)
After this, SR.UIF is set to 1...
TIM3->CNT = 0xFFFFFFFF; // let first interrupt immediately occur to immediately start ADC conversion
TIM3->CR2 |= (TIM_CR2_MMS_1); // Update event of timer will trigger TRGO
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.