2016-06-05 6:42 AM
I'm using the STM32F746G to play with some audio DSP stuff and it's working fine with headphones but when I connect the output to external amps I get whine and low signal level. I'm using the
OUTPUT_DEVICE_HEADPHONE
from the demo. I would expect it to be a fairly strong line level signal. Any tips? Thanks. P.S. I would spend more time searching this forum if it were not so painfully slow. They must be hosting on a 286.2016-06-05 1:18 PM
Still wading thru the datasheet for the WM8994 DAC but it's fairly complex. Is there any chance the headphone output is class D and the lack of an apparent signal there as a ''line output'' is due to lack of inductive/capacitive loading? What would I put in place, just a single pole LPF? 470 resistor 0.01 cap maybe and tap signal off the cap?
2016-06-06 10:40 AM
At this point I'm just presuming the audio path on this board is not super pristine. I seem to see a lot of crosstalk between the line inputs and the headphone outputs and that in turn limits my levels. So I just do a balancing act between levels and noise floor.
I'm open to suggestions/workarounds though obviously.
2017-04-16 7:42 PM
I posted this question almost a year ago. I still have low level whine in the audio output. Turning the volume for 0 for the DACs doesn't seem to affect it so it seems like it's in the hardware.
Any ideas? Anyone ever added some more uF across the power supply? Tantalum?
Dennis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.