cancel
Showing results for 
Search instead for 
Did you mean: 

LED Array question

sl1solo762
Associate II
Posted on July 10, 2011 at 21:21

I apologize if I am oversimplifying this question, but I'm on the newer side to MCU's.

   Anyways, I was trying to figure out putting together a LED array using GPIOC 8-12 and GPIOA 8-12 to make a 4x6 array. I had figured upon using a kind of row addressing to individually light the LED's in the array, but that involves being able to 'ground out' an input pin and set the other on, and vice versa to allow for (4*6)*2=48 total independent LED's. 

  Down to specifics though, if you didn't care to read the above:

If i have this

GPIOC->CRH &=0xFFFFFF0;

GPIOC->CRH |= 0x00000001; // Set pin 8 at General purpose Push/Pull

GPIOC->BSRR = 1UL<<8; // Turn on LED

and would like to, instead of grounding 8 into the GND pin on the board, ground it into GPIOC pin 9. Is there any way that is done? 

Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
sl1solo762
Associate II
Posted on July 13, 2011 at 03:38

Figured it out..  i think. So with 2  LED's, one hooked up with the cathode into my GPIOA 8 port and the anode into my 3v pin, i can enable it by setting

 GPIOA->BRR = 1UL<<8; (a crude solution)

To enable the other, with anode in the GPIO port:

GPIOA->BSRR = 1UL<<8; 

both done once the CRH is configured. 

If anyone has a better way of doing this, I'd appreciate hearing of it. I also realized that using an 8 bit shift register (serial to parallel) would give me many more possibilities for LED arrays. 

Andrew Neil
Super User
Posted on July 13, 2011 at 08:19

I hope you just omitted to mention the current-limit resistor for the sake of simplicitly/clarity...?

Also, in addition to the port pin current limit, remember that there is a limit to the total current through all pins of a port, and also a limit to the total current through all pins of the package.

You cannot drive all pins simultaneously to the per-pin  maximum...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.