2024-11-17 3:39 AM
I have a bit of code as follows:
str r3, [r0, #68]
ldr r3, [r0, #68]
where [r0, #68] is TIM20.BDTR on a STM32G474. I would expect that the LDR would output the same data that was just stored, however it seems that out outputs the previous data. I also tried putting a DMB between the two instructions but the same result still occurred. Inserting 5 DMB instructions seems to cause a long enough delay that the correct data is returned.
This obviously has the potential to be problematic in a few scenarios, but I can't find any documentation from ST on this behaviour, so does anyone know if such documentation exists?
Solved! Go to Solution.
2024-11-17 10:55 AM
Hi @liampwll ,
That is the best workaround :
80128b4: 6c43 ldr r3, [r0, #68] @ 0x44
80128b6: 6c43 ldr r3, [r0, #68] @ 0x44
Just doing a dummy Read back after the first store ! the second LDR will have the right store value.
Cheers,
STOne-32.
2024-11-17 3:49 AM
Never mind, it turns out this is just another case of a key detail being buried in an obscure part of the reference manual:
Because MOE falling edge can be asynchronous, a resynchronization circuit has been inserted between the actual signal (acting on the outputs) and the synchronous control bit (accessed in the TIMx_BDTR register). It results in some delays between the asynchronous and the synchronous signals. In particular, if MOE is set to 1 whereas it was low, a delay must be inserted (dummy instruction) before reading it correctly. This is because the write acts on the asynchronous signal whereas the read reflects the synchronous signal.
- RM0440 Rev 8 28.3.18
However, this still seems to be wrong as a single DMB does not seem to be a long enough delay, so does anyone know what the actual required delay is?
2024-11-17 4:21 AM
Dear @liampwll ,
That register is on APB2 bus, interpretation of cycle is based on it’s own cycles . So if for example the AHBtoAPB2 ratio clock is 4 . One APB2 cycle means 4 AHB or CPU cycles etc.
DMB is acting only at CPU Cortex / AHB cycle to wait till the Internal Cortex-M prefetch is flushed and can not help to wait the APBs mapped registers thru the Bridges . Do you know your AHB/APB2 configuration? And if inline with inserting dummy Reads after the STORE ?
Let us know .
STOne-32
2024-11-17 4:50 AM - edited 2024-11-17 4:52 AM
They're both /1 (HPRE = 0, PPRE = 0). The following works as expected rather than using a DMB, so something about DMB causes an issue even though it should cause at least a single cycle wait as far as I'm aware:
80128ac: 6c43 ldr r3, [r0, #68] @ 0x44
80128ae: f443 4300 orr.w r3, r3, #32768 @ 0x8000
80128b2: 6443 str r3, [r0, #68] @ 0x44
80128b4: 6c43 ldr r3, [r0, #68] @ 0x44
80128b6: 6c43 ldr r3, [r0, #68] @ 0x44
80128b8: 041b lsls r3, r3, #16
2024-11-17 10:55 AM
Hi @liampwll ,
That is the best workaround :
80128b4: 6c43 ldr r3, [r0, #68] @ 0x44
80128b6: 6c43 ldr r3, [r0, #68] @ 0x44
Just doing a dummy Read back after the first store ! the second LDR will have the right store value.
Cheers,
STOne-32.
2024-11-27 9:23 PM
@STOne-32 Could you suggest to the docs team that the register definitions really need some sort of indication when a read is not guaranteed to be equal to the previous write? Even if it's just an asterisk next to the field name without any further details, it would be incredibly helpful to not get caught out by things like this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.