2023-12-14 6:08 AM
Hello everyone
i've been trying to use FMAMSDXX015WCSC3 force sensor. sensor address 0x28 and whenever i was trying to do IsDeviceReady function, its been always keep getting me HAL_Busy.
HAL_StatusTypeDef status = HAL_I2C_IsDeviceReady(&hi2c2, 0x28 << 1, 10, 2000);
delay(250);
if (status == HAL_OK ){
HAL_Delay(5); //making the status dont be optimized out.
}
And also when i'm using external or internal(in GPIOInitStruct.Pull) pull up resistor that
function giving me a HAL_ERROR. So is my sensor broke or am i doing something wrong?
Down there, there is the my peripherals created by CubeIde.
void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hi2c->Instance==I2C2)
{
/* USER CODE BEGIN I2C2_MspInit 0 */
/* USER CODE END I2C2_MspInit 0 */
__HAL_RCC_GPIOB_CLK_ENABLE();
/**I2C2 GPIO Configuration
PB10 ------> I2C2_SCL
PB11 ------> I2C2_SDA
*/
GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* Peripheral clock enable */
__HAL_RCC_I2C2_CLK_ENABLE();
void MX_I2C2_Init(void)
{
/* USER CODE BEGIN I2C2_Init 0 */
/* USER CODE END I2C2_Init 0 */
/* USER CODE BEGIN I2C2_Init 1 */
/* USER CODE END I2C2_Init 1 */
hi2c2.Instance = I2C2;
hi2c2.Init.ClockSpeed = 100000;
hi2c2.Init.DutyCycle = I2C_DUTYCYCLE_2;
hi2c2.Init.OwnAddress1 = 0;
hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c2.Init.OwnAddress2 = 0;
hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C2_Init 2 */
/* USER CODE END I2C2_Init 2 */
}
2023-12-14 7:24 AM
Is FMAMSDXX015WCSC3 the correct part number for your part?
Looking at a datasheet:
FM = MicroForce Sensors
A = Compensated / Amplified
M = Mechanical
S = Sphere
D = Sensor Short and Open
XX = Future Placeholder
015 = 15 Newtons
W = Newton
C = Compression
S = SPI
C = Transfer Function
3 = 3.3V
This would suggest its an SPI interface (rather than I2C)?
2023-12-14 7:45 AM
Also, don't use the internal pull-ups - use proper external pull-up resistors (10K should be fine).
2023-12-14 9:23 PM
when copying from datasheet i was copied wrong name it is FMAMSDXX015WC2C3 sorry to missleading you. 2 means ı2c 0x28.
2023-12-14 9:24 PM - edited 2023-12-14 10:27 PM
Well, in the datasheet, it said 1k is enough, and I used a 2.2k resistor. I should change it, I guess. And 10k doesn't work. And when I am using a pull-up resistor, it still gives me a HAL_ERROR. I guess my sensor has been broken. So, are there any other things I should try? It was an expensive sensor, and I don't want to throw it away if I'm not 100% sure it's broken.
2023-12-15 6:58 AM
10K is fine for normal applications at 100 kHz. Post a schematic. Get a scope on both SCL and SDA.
2023-12-15 5:48 PM
...it still gives me a HAL_ERROR. I guess my sensor has been broken. So, are there any other things I should try?
A beginner code based on the HAL broken bloatware is not an indicator of hardware flaws or basically anything. You can try learning and developing a decent code.
2023-12-18 1:44 AM
As @David Littell suggested you need to go through the "Physical" board level stuff first to satisfy yourself that that is all correct. Some suggestions below:
These little steps may not solve your problem yet, but it builds more confidence on what the problem isn't.
Note: You may have done these already, but without knowing the answer to these its hard to say if the device is "broken" unless you know that there's a chance it probably is for some reason.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.