2025-07-13 3:54 PM - edited 2025-07-13 4:16 PM
Hi,
I'm configuring the independent watchdog in the STM32F103xx medium-density using the registers.
During the IWDG the PVU bit is not cleared by the hardware. The reference manual (page 498) says the following:
"PVU: Watchdog prescaler value update
This bit is set by hardware to indicate that an update of the prescaler value is ongoing. It is
reset by hardware when the prescaler update operation is completed in the VDD voltage
domain (takes up to 5 RC 40 kHz cycles).
Prescaler value can be updated only when PVU bit is reset."
RCC->CSR |= (0x1 << 0); // Enable LSI
while (!(RCC->CSR & (0x1 << 1))); // Wait for the LSI to be ready
IWDG->KR = 0x5555; // unlock PR and RLR
IWDG->PR = 0x3; // Divided by 32
IWDG->RLR = 0xFFF; // 4096 - counter value
while (IWDG->SR & (1 << 0)); // PVU <- #### GET TRAPPED IN HERE ####
while (IWDG->SR & (1 << 1)); // RVU
IWDG->KR = 0xAAAA; // reload the counter
IWDG->KR = 0xCCCC; // start IWDG
Debugging using GDB, the RCC bits are correct, LSI is activated and being used, the 0xFFF value in IWDG->RLR is set, but the prescaler value (0x3) in IWDG->PR is not being set because the PVU bit is not being reseted.
Solved! Go to Solution.
2025-07-13 7:04 PM
It may need started before the registers are updated. That's what HAL does.
2025-07-13 7:04 PM
It may need started before the registers are updated. That's what HAL does.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.