2013-10-04 7:00 AM
Hi All,
i'm using STM32F407, USB Device library V1.1.0 / 19-March-2012, i'm able to receive from PC to STM bytes using CDC, but i'm unable to send to PC from STM :( i modified function like this : static uint16_t VCP_DataTx (uint8_t* Buf, uint32_t Len) { for( uint16_t i = 0; i < Len; i++) { APP_Rx_Buffer[APP_Rx_ptr_in] = CDCdebug_tx_buf[ i ]; APP_Rx_ptr_in++; /* To avoid buffer overflow */ if(APP_Rx_ptr_in == APP_RX_DATA_SIZE) { APP_Rx_ptr_in = 0; } } CDCdebug_tx_buf_len=0; return USBD_OK; } most of lines was taken from CDC template from Library, thanks for all replies, Kind regards, UPDATE: i forgot to call that function ... it's not called by any Handler as i thought, please remove topic ...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.