STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Parallel output of 8bits

Posted on October 04, 2013 at 11:13I have found working solution. But for me it look ugly.uint8_t command = 0x55; uint16_t u16Temp = 0; u16Temp = GPIO_ReadOutputData(GPIOA)&0xFF00; u16Temp |= command; GPIO_Write(GPIOA, u16Temp); Is there better way ...

pchala by Associate II
  • 1852 Views
  • 3 replies
  • 0 kudos

STM32L151RD inexplicable/weird crash

Posted on October 03, 2013 at 17:15 Hi, I developed an application using the STM32L152D Evaluation board and everything was working as expected. The application was then moved to the actual project which uses a STM32L151RD microcontroller...

andrei by Associate II
  • 3236 Views
  • 7 replies
  • 0 kudos

DMA and two or more U(S)ARTs

Posted on October 03, 2013 at 09:50Can I configure two usart's to use one DMA? In datasheet there is table called ''DMAx request mapping'' and for stm32f40/1/2/3 eg. UART4 uses channel 4 for RX and TX DMA trigger on stream 2 and 4. Can I configure s...

pawwodko by Associate II
  • 1597 Views
  • 3 replies
  • 0 kudos

STM32 F0 hangs when using USART & interrupts

Posted on October 04, 2013 at 04:46Hi, I'm trying t owrite robust code for USART communication with embedded modem like module. Since communication is not strict command-response manner, but module can send messages also in asynhrounous manner (spor...

STM32F407 DMA USART Issue?

Posted on September 20, 2013 at 17:30Hello, I am using a STM32F407. My application needs both USART1 and USART6 to concurrently receive data. I would like to use DMA2 to transfer data received from each USART to external RAM via the FSMC and ensure...

jnalasco by Associate
  • 2193 Views
  • 4 replies
  • 0 kudos

timer TIM2 to TIM5 behavior, stm32f4 discovery board

Posted on September 30, 2013 at 13:14 hello all and thanks for your help, I'm working with stm32f4 discovery board and I will like to use two different timers. For the timer TIM3 after a long work I set certain parameters so I can have my des...

jpablo by Associate II
  • 3930 Views
  • 8 replies
  • 0 kudos

Development tool for STM32F4

Posted on October 01, 2013 at 08:03Hello      I am Working with STM32F4 Discovery since couple of months.I have tried few basic program with this and now trying  to do some more advance assignments like USB serial,CAN implementation with STM32F4 Dis...

Stm32L151rct6a EXTI Configuration Hang Problem

Posted on October 03, 2013 at 08:47STM32L151RCT6A under IAR Compiler, board hangs when I do these steps  /* Enable SYSCFG clock */  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);  /* Connect EXTI1 Line to PA9 pin */  SYSCFG_EXTILineConfig(EX...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.