2024-11-28 5:04 AM - edited 2024-11-28 5:11 AM
Hello all,
I developed a UDP server/client with the objective to send and receive data simultaneously. The code has some problems in the way its written (e.g., unnecessary loops, variable definitions inside a loop...), but I'm only interested in solving one problem which is the amount of data I'm able to send from my stm32 to my pc, I want to send 3 TS packets at a time (188*3=564 bytes per UDP transmission), but the maximum number of bytes i was able to transmit is 209 bytes, if i make it 210 bytes, I receive nothing on my PC (python).
The basic flow of the data I want to send is:-
I'm initializing three buffers with TS headers:
uint8_t uart2_data[188] = {0x47, 0x1F, 0xFF, 0xD0, 0x03};
uint8_t uart1_data[188] = {0x47, 0x1F, 0xFF, 0xD0, 0x01};
uint8_t uart6_data[188] = {0x47, 0x1F, 0xFF, 0xD0, 0x02};
Then, to each buffer i will add "additional_data" to create a TS packet:
uint8_t additional_data[183] = {
'H', 'e', 'l', 'l', 'o', ' ', 'W', 'o', 'r', 'l', 'd', // ASCII text "Hello World"
'A', 'B', 'C', 'D', 'E', 'F', 'G', 'H', 'I', 'J', 'K',
'L', 'M', 'N', 'O', 'P', 'Q', 'R', 'S', 'T', 'U', 'V',
'W', 'X', 'Y', 'Z', 'a', 'b', 'c', 'd', 'e', 'f', 'g',
'h', 'i', 'j', 'k', 'l', 'm', 'n', 'o', 'p', 'q', 'r',
's', 't'
};
memcpy(uart2_data + 5, additional_data, 183);
memcpy(uart1_data + 5, additional_data, 183);
memcpy(uart6_data + 5, additional_data, 183);
After that, I will store each TS packet to one buffer (message_with_counter):
snprintf(message_with_counter, sizeof(message_with_counter), "%s%s%s", uart2_data, uart1_data, uart6_data);
The whole UDP client functions:
// Initialize the UDP client to communicate with PC
void udpClient_init(void)
{
err_t err;
/* 1. Create a new UDP control block */
client_upcb = udp_new();
/* Bind the block to STM32 IP and port */
ip_addr_t myIPaddr;
IP_ADDR4(&myIPaddr, 192, 168, 1, 90); // STM32 client IP address
// udp_bind(client_upcb, &myIPaddr, 9); // Port 8 for client
/* Configure destination IP address and port (PC server IP and port) */
ip_addr_t DestIPaddr;
IP_ADDR4(&DestIPaddr, 192, 168, 1, 20); // PC server IP
err = udp_connect(client_upcb, &DestIPaddr, 61000);
if (err == ERR_OK)
{
udp_recv(client_upcb, udp_receive_callback, NULL); // Set receive callback
udpClient_send(); // Start sending messages
}
}
// Function to send data from UDP client to server (PC)
void udpClient_send(void)
{
//struct pbuf *txBuf;
char message_with_counter[564]; // Buffer to hold the final message with counter
while (1)
{
//struct pbuf *txBuf;
struct pbuf *txBuf;
//char message_with_counter[564];
uint8_t uart2_data[188] = {0x47, 0x1F, 0xFF, 0xD0, 0x03};
uint8_t uart1_data[188] = {0x47, 0x1F, 0xFF, 0xD0, 0x01};
uint8_t uart6_data[188] = {0x47, 0x1F, 0xFF, 0xD0, 0x02};
uint8_t additional_data[183] = {
'H', 'e', 'l', 'l', 'o', ' ', 'W', 'o', 'r', 'l', 'd', // ASCII text "Hello World"
'A', 'B', 'C', 'D', 'E', 'F', 'G', 'H', 'I', 'J', 'K',
'L', 'M', 'N', 'O', 'P', 'Q', 'R', 'S', 'T', 'U', 'V',
'W', 'X', 'Y', 'Z', 'a', 'b', 'c', 'd', 'e', 'f', 'g',
'h', 'i', 'j', 'k', 'l', 'm', 'n', 'o', 'p', 'q', 'r',
's', 't'
};
memcpy(uart2_data + 5, additional_data, 183);
memcpy(uart1_data + 5, additional_data, 183);
memcpy(uart6_data + 5, additional_data, 183);
// Receive data from UART2 (Docklight) into the uart2_data buffer
// HAL_UART_Receive(&huart2, uart2_data + 5, 183, 1000); // Timeout of 10ms
// HAL_UART_Receive(&huart1, uart1_data + 5, 183, 10); // Timeout of 10ms
// HAL_UART_Receive(&huart, uart6_data + 5, 183, 10); // Timeout of 10ms
snprintf(message_with_counter, sizeof(message_with_counter), "%s%s%s", uart2_data, uart1_data, uart6_data)
// Prepare the UDP pbuf with the message with counter
txBuf = pbuf_alloc(PBUF_TRANSPORT, strlen(message_with_counter), PBUF_RAM);
if (txBuf != NULL)
{
/* Copy message with counter to pbuf */
pbuf_take(txBuf, message_with_counter, strlen(message_with_counter));
//pbuf_take(txBuf, message_with_counter, sizeof(uart2_data) + sizeof(uart1_data) + sizeof(uart6_data));
/* Send UDP data */
udp_send(client_upcb, txBuf);
/* Free the pbuf */
pbuf_free(txBuf);
osDelay(15);
}
}
}
My question is: What causes the limitation or constraint to be 209 bytes per UDP transmission?
2025-01-14 8:18 AM
Hello @CosmicWreck ,
this is clearly not a limitation of an ST product even if you are not specifying which series running what code with the Firmware version used and tools (IAR ,CubeIDE , Keil).
I recommend you start by referring to examples and also see this article which may help you implement this correctly.
Regards
2025-01-14 8:23 AM
@CosmicWreck wrote:if i make it 210 bytes, I receive nothing on my PC (python).
Are you sure that's an issue on the STM32? Maybe it's on the PC end ...
Have you used Wireshark (or similar) to see what's actually happening on the wire ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.