2023-07-13 5:30 AM
I am currently working on a project that involves reading PDM (Pulse-Density Modulation) data from a digital MP34DT06J microphone and converting it to PCM (Pulse Code Modulation). However, I am encountering difficulties when attempting to read data from the PDM buffer using SAI (Serial Audio Interface).
To provide some context, I have successfully tested the microphone using the I2S (Inter-Integrated Sound) interface, where everything works as expected. However, when I switch to the SAI interface, I am unable to read any data from the PDM buffer.
Here are the specifics of my setup:
Despite configuring the SAI interface according to the relevant specifications, I am still unable to retrieve any data from the PDM buffer. I have double-checked the connections and reviewed the documentation, but I have not been able to identify the root cause of this issue.
If possible, I would greatly appreciate it if someone could provide an example or code snippet demonstrating the correct setup and configuration of the MP34DT06J microphone with the SAI interface. This would greatly help me in resolving the problem and understanding any potential errors I may have made in my implementation.
Thank you in advance for your assistance. I look forward to your valuable input.
2023-07-13 8:04 AM
You should post the relevant code snippets here:
- SAI init
- DMA init
- buffer init
- SAI / DMA start
- IRQ handlers
2023-07-17 4:28 AM
Hey! @LCE, I'm attaching the code main.c file below. Please have a look.
Also, the MX_PDM2PCM_Init function definition is given below for reference.
void MX_PDM2PCM_Init(void)
{
PDM1_filter_handler.bit_order = PDM_FILTER_BIT_ORDER_LSB;
PDM1_filter_handler.endianness = PDM_FILTER_ENDIANNESS_BE;
PDM1_filter_handler.high_pass_tap = 2104533974;
PDM1_filter_handler.in_ptr_channels = 1;
PDM1_filter_handler.out_ptr_channels = 1;
PDM_Filter_Init(&PDM1_filter_handler);
PDM1_filter_config.decimation_factor = PDM_FILTER_DEC_FACTOR_64;
PDM1_filter_config.output_samples_number = 16;
PDM1_filter_config.mic_gain = 24;
PDM_Filter_setConfig(&PDM1_filter_handler, &PDM1_filter_config);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.