2019-01-21 5:24 AM
hello,
Iam having a issue in uploading the code to STM32F100ZC, I have attached the schematic of SW interface done. Its showing an error that target is not connected. I have done all the possible connections for BOOT0 and BOOT1 pins.
Please help me solve it.
Thank you
2019-01-21 5:56 AM
Perhaps the part isn't actually functioning?
Check orientation
Check pin state of NRST
Check voltage on VDDA
Make sure a stand-alone ST-LINK has both 3V3 and GND connected
Check ST-LINK with ST-LINK Utilities
Make sure you have correct debugger selected in Keil, and it can see device
Try using USART1 PA9/PA10, BOOT0 High, Reset, Send an 0x7F byte at 9600 8E1, check for 0x79 response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.