STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am trying to use I2C communication using ST NUCLEO-F030R8 with AT24C64 and modifying code generated by STM32CubeMX. When I use HAL_I2C_IsDeviceReady function it returns HAL_OK but HAL_I2C_Mem_Write or HAL_I2C_Mem_Read function returns error

if(HAL_I2C_IsDeviceReady(&hi2c2,0xA0,10,100)==HAL_OK){ sprintf((char*)TxBuff,"\r\ni2c device ready");}else{ sprintf((char*)TxBuff,"\r\ni2c device fail");}if(HAL_I2C_Mem_Write(&hi2c2,0xA0,mem_add,32,&data_send,1,10)==HAL_OK){ sprintf((char*)TxBuff,"\r...

NAmat by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos

UART tx stop when I send messages for a long time

I'm using uart fuctions with my board STM32F401RE.I don't use cts, rts (hardware flow control) and any receiving process.So I only transmitt some values to PC but I found that when I send a message constantly, suddenly it stop. I think it's related w...

dlee.0 by Associate II
  • 1879 Views
  • 3 replies
  • 0 kudos

Install DFU driver on Win7 failed

Posted on August 11, 2015 at 04:28Hi guys,I wanted to test DFU function with my STM32F401 board, and my Win7 has installed DfuSe V3.0.4. After I plug USB to PC, it shows the driver is not corrected, so DfuSe can't recognized the USB device.I searche...

dqyang by Associate II
  • 6414 Views
  • 13 replies
  • 0 kudos

USB CDC -- zero length packets

Posted on May 25, 2016 at 23:27I used stm32cubeMX to generate a CDC project for the stm32f3 discovery board.  After much fussing, I have a pretty stable echo going.  If I use a program to generate output/input from the host, I'm finding writes of 64...

Issue with using internal opamp on the STM32L4

Hi I have been reading an ST presentation regarding using the internal opamp on a STM32L433. Am I reading it correctly, this saves in having to use an external opamp? I want to use it for as a follower for the analogue input. I am not sure I am read...

can we run multiple applications same time on stm32

Hi, I want to run DSP lowpass filter and also run other applications like voice over ble and touch screen interrupts at the same time. running one after the other is not efficient.Is there a way to run these applications in parallel on a stm32 proces...

VPotl by Associate II
  • 3737 Views
  • 6 replies
  • 0 kudos

Resolved! reset all MAC subsystem internal registers and logic - fail?

DMABR->SR should be auto-cleared when set 1.I haven't modified code - auto generated by hal.It always timeouts - any ideas why? I tried to extend timeout time - bit 0 is always 1.Here is code from HAL: /* Ethernet Software reset */ /* Set the SWR ...

John Doe1 by Associate III
  • 1649 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.