2020-01-22 2:49 AM
I am programming the uC via UART that is connected via a Transceiver. The transceiver has an DE (Driver Enable) pin which is active high. Unfortunately, it has a pull down instead of pull-up in a design, therefor the uC can hear but can't talk back. This pin (DE) is also connected to one of the uC GPIOs. If only I could set this pin high by sending something to the uC when its in the boot-loader mode.., can I?
Other thought would be to force the STM32Cube to connect.. as off it has received the 0x7F from the uart.
Please help.
2020-01-22 3:07 AM
> Is there any way to set a specific GPIO high when entered a bootloader
No. You have to fix the hardware.
JW
2020-01-22 3:45 AM
If you mean the ROM-based system bootloader, the answer is no.
But perhaps you can override the DE pin of your transceiver module with a pull-up, which you can later disable (or reset) from within your application.
Or skip the system BL alltogether, and use your own.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.