2024-11-18 12:29 PM - last edited on 2024-11-19 1:21 AM by Andrew Neil
2024-11-19 2:37 AM
There's no need to format your whole post as BOLD!
Yes - as the name suggests, the STM32CubeIDE is for the whole STM32 product range.
2024-11-18 1:56 PM
Yes, there is at least one. Can you guess which? ))
2024-11-18 2:26 PM
Cubemx and Cubemx IDE???
I have been using both for Nucleo STM32C0.
2024-11-18 3:37 PM
What does the Product Page tell you ... ?
https://www.st.com/en/evaluation-tools/nucleo-h753zi.html#tools-software
2024-11-18 4:01 PM - last edited on 2024-11-19 1:21 AM by Andrew Neil
Thanks Andrew,
There are two choices below - Should I choose the first one - "Patch_CubeH7"???
1. Patch_CubeH7
2. STM32CubeH7
Thanks again!!!
2024-11-19 1:28 AM
No, there is only one IDE listed there:
As the name suggests, STM32CubeIDE is the IDE.
@RongShengWang wrote:Patch_CubeH7
It's "Pack" - not "Patch".
As it says. it's a software pack with the HAL drivers, etc:
https://www.st.com/en/embedded-software/stm32cubeh7.html
You use that in conjunction with the IDE of your choice.
With CubeIDE, you don't need to download it separately - CubeIDE will download it for you when you start a Project.
2024-11-19 2:33 AM
Thanks.
I have been using Cubemx and Cubemx IDE for Nucleo STM32C0. board.
The IDE should be the same for STM32H7, right? Thanks!
2024-11-19 2:37 AM
There's no need to format your whole post as BOLD!
Yes - as the name suggests, the STM32CubeIDE is for the whole STM32 product range.
2024-11-19 9:49 AM
For the STM32C0, and ALL STM32 CM0(+) there's also a free KEIL MDK Licence available.
Doesn't work with CM3/CM4/CM7 cored parts
2024-11-19 10:35 AM
free KEIL MDK Licence doesn't work with CM3/CM4/CM7 cored parts - right?
Thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.