2022-05-05 12:31 AM
I would like to build an application on an STM32 microcontroller (the one integrated in the NUCLEO-L432KC) that allows to transmit a message of 192 bytes or more if possible on CAN BUS.
At first, I was thinking of a mechanism that in the transmission phase allows me to divide the data into several 8-byte messages and then on the receiving side an inverse mechanism that allows me to reconstruct it. However, I came across an article that talks about ISO 15765-2 CAN-TP Protocol which is an international standard protocol used for sending more than 8-bytes of data over the CAN consecutive frames. Is there an ST API that implements this protocol?
Thank you in advance!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.