2018-08-20 3:50 AM
Hi,
I have read a few forum posts on here with regards to STM32's working with specific USB PHYs. There is a lot of confirmation that the MicroChip USB3320 works with specific STM32's. In fact the dev kit for the STM32H743 (which is the Micro I am using) has a USB3320 on it.
My question is:
Why aren't the ST ULPI USB PHYS, STUPLI01, on the ST dev kits?
Is the STUPLI01 compatible with the STM32H743, for HS USB data transfers?
Thanks in Advance,
Jack
2018-10-01 1:55 AM
I think your question is a rightful one and I wonder the same thing.
I can tell tou that I have a design with an STM32F7 and an STULPI01B that works fine.
Actually I have some stall issues during long streams, but I think they are closely related to my hardware configuration.
2019-04-08 3:11 AM
Hi LoriB,
Thanks for your answer.
I finally have some PCBs with the ST32 and the PHY on but we are having trouble deciphering the software commands to put the PHY into HS Peripheral mode.
From what I can tell I need to write data 0x40 to the Function Control register and data 0x00 to the OTG register.
I am confused by the addresses of these registers though:
The Function Control register for example (Pg 32 of the datasheet) states:
Read (04H-06H),
Write (04),
Set (05),
Clear (06)
How can read cover all the addresses - how do we differentiate between a read and a write for example?
I have seen that, you must put a TXCMD on the ULPI data pins (0x10XXXXXX for read and 0x11XXXXXX for write)
But why does Figure.10 High-speed mode entry show 0x84, 0x50 being written to the ULPI?
I have to admit I find the datasheet for this device incredibly difficult to follow!
Could you please help me to understand this better?
Thanks,
Jack
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.