2022-01-19 1:41 AM
I am trying to configure the SAI block in slave mode to receive a set of data. The Frame Sync signal and the data clock shall be provided from an external device. In a case where the active frame length and the frame length are to be decided by the master device, is it necessary that these parameters are configured during initialization of the block? If yes, is there a default value that is to be provided ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.