STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F030C8T6TR Reset continuesly time interval?

I place oscilloscope probe at reset pin of MCU it get low reset continuously time period​I observed RCC​- CSR resistor which gives LSIRDY=1 AND IWDGRSTF=1 both are set How can I make them of and solve this reset problem?​Below attached images of MCU ...

0693W00000JMK8UQAX.jpg 0693W00000JMK8PQAX.jpg

Resolved! Best way to use DMA without knowing size of SPI transfer ?

Hi,device : STM32G473VBT6What is the best way to process SPI data when we don't know how many bytes will come from the SPI master ?I use the SPI in full duplex slave.The problem with DMA is that the DMA buffer is circular, where my processing functio...

sde c.1 by Senior II
  • 6555 Views
  • 9 replies
  • 0 kudos

Is the parameter 'ActiveFrameLength' and 'FrameLength' under the FrameInit significant when the SAI module is configured to operate in slave mode to receive data?

I am trying to configure the SAI block in slave mode to receive a set of data. The Frame Sync signal and the data clock shall be provided from an external device. In a case where the active frame length and the frame length are to be decided by the m...

Jansunil by Associate II
  • 933 Views
  • 0 replies
  • 0 kudos

Updating the firmware on my STM32H745ZI-Q causes CPU2 not to boot and times out in error_handler(). Is there a way to use an older firmware?

I have updated the firmware on my STM32H745ZI-Q and when I run in debug mode the code runs until:while((__HAL_RCC_GET_FLAG(RCC_FLAG_D2CKRDY) != RESET) && (timeout-- > 0)); if ( timeout < 0 ) { Error_Handler(); }The code stops in the error handler.Is ...

KSOdin2 by Associate III
  • 1064 Views
  • 2 replies
  • 0 kudos

Resolved! Fails to execute from QSPI Flash but read works

Hi,I have some issues with executing directly from QSPI with a NUCLEO-F412ZG and a connected Winbond W25Q80DV QuadSPI Flash which we are looking into as a workaround for the component shortage (will be a L4 variant but using a F4 for testing).Reading...

HSE oscillator when using USB

The STM32F303xB datasheet states that HSE oscillator should be used when using USB. I suspect it is because of the degraded accuracy of the HSI oscillator at temperature. I've had issues with CAN not working well with HSI at elevated temperature. Doe...

Resolved! Problem in using flash memory of STM32H745

MCU : STM32H745Boot : booting from user main memory(0x08000000 )of flash memory ( boot0 :low)compiler: IAR​I am coding to write in address 0x08060000 of flash memory in Cortex M7 . Cache is enabled, MPU is configured below After at first writing 4444...

0693W00000JMSgUQAX.png 0693W00000JMShwQAH.png 0693W00000JMSkRQAX.png 0693W00000JMSpHQAX.png
hryu.1 by Associate II
  • 1311 Views
  • 1 replies
  • 0 kudos

Resolved! SPI1 SCK Polarity is incorrect.

I have a B-U585I-IOT02A Discovery board, which is connected it to an external ST LSM6DS3 accelerometer via the SPI1 pins on the arduino connector. The issue is that the SCK line is going low when not active even though I have it configured to be hig...

0693W00000JMQfaQAH.jpg 0693W00000JMQjCQAX.jpg
cBroadbo by Associate II
  • 2041 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.