2015-09-09 11:03 PM
Can anyone tell me if a SPI driver exists to link with FATFs that supports SDHC/SDXC cards. i.e. greater than 4GB.
The examples supplied in the STCube only seems to support SDSC <4GB.I see that clive1 has patched the SDIO example in the link below but I am looking for a SPI version.https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FSTM32%20sdio%20sdhc%204gb%20problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=6546If it doesn't exist then I will have to patch the existing example but I would obviously like to avoid this.I am developing on the STM32F030R8-Discovery which uses the stm32_adafruit_sd.c driver to interface with the FATFs as starting point.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.