2024-04-15 10:24 AM - edited 2024-04-15 10:35 AM
Hi,
i know the gotcha about the late clearing. My interrupt (yes it currently useless) is so short, that clearing in the beginning would not work either, so i tried to implement a check for the interrupt flag. But with no success: It is fired twice.
Is my approach wrong?
This is the interrupt:
/*
* Exiting interrupt with if(true)+(2 NOP´s) is about 20ns, Checking for "! (TIM8->SR & TIM_SR_COMIF)" adds 120ns!
*/
void TIM8_TRG_COM_IRQHandler(){
GPIOC->BSRR = (uint32_t) GPIO_PIN_3;
if(! (TIM8->SR & TIM_SR_COMIF)){ // Return if no flag is set (prevents false triggers because of latency in the bus)
__ASM volatile ("NOP");
__ASM volatile ("NOP");
GPIOC->BRR = (uint32_t) GPIO_PIN_3;
return;
}
TIM8->SR = ~TIM_SR_COMIF; // DONT send "&=" ReadModifyWrite is bad!
__ASM volatile ("NOP");
__ASM volatile ("NOP");
GPIOC->BRR = (uint32_t) GPIO_PIN_3;
}
2024-04-15 10:37 AM
How do you measure? The PC3 signalling would presumably look very similar on either branch.
Perhaps use a proper memory fencing operation instead of the NOP's ? Could you use __DSB(); ?
>>Is my approach wrong?
If it's not working, and you're looking at right problem, probably..
Look at other causes for TIM8_TRG_COM_IRQHandler() might be entering. What's TIM8->SR flagging
How many times is it entering with no interrupt source flagging?
Approach the problem from understanding of WHAT is actually happening, not applying random remedies until it stops.
2024-04-15 1:15 PM - edited 2024-04-15 1:16 PM
This is a bit embarrassing:
After working with a 600 bucks scope, that rather confuses than helps, having manuals that do also a fair bit of confusing and having to little breaks, i was not able to understand, that it actually does what i wrote it to do.
I have read about the __DSB(), that it is rather not reliable. There would be other structures, that would interfere and prevent to work the right way. (http://efton.sk/STM32/gotcha/g7.html)
2024-04-15 2:03 PM
Checking the flash won't prevent the interrupt to fire twice. It prevents the relevant content if interrupt to be executed twice.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.