STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Speed UART transmissions using HAL_UART_Transmit_IT() vs I2C

I detected that transmitting 68 characters using RS232 at 460800hz takes 30-32000 tics to micro running at 480Mhz (HAL_UART_Transmit() takes 10 times more).Is there a method to disturb less to micro to make that transactions, perhaps using DMA?Is bet...

JLope.11 by Associate III
  • 824 Views
  • 0 replies
  • 0 kudos

Resolved! COM update interrrupt is delayed 1.3us

Hi,i am trying to figure out, why this interrupt is delayed that much.The com trigger comes from timer 1, which works as expected. Also the delay here is as expected too (apart from a 50ns deviation). There is a delay of 1.3us, from the time i can ob...

Tobe by Senior III
  • 6108 Views
  • 8 replies
  • 2 kudos

Resolved! Function return value problem to the FreeRTOS task

Hi All!I'm doing a project on the STM32F429 discovery board.In this project, I've used the TouchGFX.Also, I'm using the FreeRTOS. The idea is to read the Temperature sensors and read their values to the TextAreas in TouchGFX.TouchGFX was tested and w...

Analyzer_Cmd.png Analyzer_Data.png
USolar by Associate III
  • 6378 Views
  • 3 replies
  • 2 kudos

Are there any documentations about FSMC layout?

I am now designing a board for STM32F103VET6 and would like to use the FSMC to control the TFT LCD (320x480 resolution)May I ask if there are any notes or guides that mention the layout requirements? Such as what conductor impedance should the data l...

OW1TY2 by Associate II
  • 2905 Views
  • 4 replies
  • 0 kudos

Resolved! VREF+ exceeding VDDA during power on/off

I'm trying to understand the following excerpts from the STM32L476 datasheet, which seem to contradict:In Table 20 - the absolute maximum voltage on the VREF+ pin is given as 4.0V (VREF+ I assume falls under the "other" category). Table 76 seems to i...

stevedebonis_0-1712092530973.png stevedebonis_1-1712092587951.png

How to connect a STM32F4xxxRE on a custom PCB

Hello,This is the first time I've designed a PCB with a stm32. I found a PDF on the internet that gives me an example of a Nucleo connection but I'm not sure if my schematic is correct.I don't need all the headerts or the usb connection (I'll be usin...

Paulo971_0-1712943662324.png Paulo971_1-1712943686124.png
Paulo971 by Associate III
  • 5662 Views
  • 10 replies
  • 4 kudos

STM32U535 Backup registers access wait states

Hi all, I am running into an issue related to writing backup registers on the STM32U535xx MCU. When I compile my code with -Oz, the write fails, whereas with -Os, it succeeds. The relevant C code is pretty straightforward:LL_PWR_EnableBkUpAccess();LL...

notepad_0swXgaLMqa.png
GeertL by Associate II
  • 2588 Views
  • 4 replies
  • 1 kudos

Program stm32F745 via RS-485 and bootloader

Hello everyoneIs it possible to program my STM32F745 via RS-485 using the integrated bootloader?My idea is using USART1 (as written in the AN2606) and a transceiver to do that. Has anyone done something similar? Thank you very much in advanced. Best ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.