2012-11-02 6:51 AM
Hello guys,
I have been messing with interrupts recently and I have hard time to find in the manuals how the priorities actually work. I have seen the priority groups and priority values. If I understood it properly, lower priorities will give the higher priority level. Though to put it in a simple situation. lets says That I have and interrupt that 'll call IRQ1 here coming every 100ms and that it's processing is lasting 20ms. Now lets say that I have an other IRQ called IRQ2 coming every 5 millisecond and lasting 1ms. If IRQ2 has a higher priority than IRQ1, does this mean that IRQ2 can be fired several times withing the processing of IRQ1 ? when IRQ2 is finished within IRQ1 processing, is IRQ1 processing resumed ? If you have further links describing the whole priority concept, thanks to point them out. I have looked into both reference manual and programming manual, but that doesn't look very clear to me :) Thanks for any clarification. Lionel #nvic2012-11-02 11:02 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.