2013-03-25 12:53 AM
hi
i am new to stm32f4. i want to read and write data to the internal sram (4kb). i am using mdk arm for compiling c code.
regards
2013-03-25 4:54 AM
The battery backed up regions?
I'd imagine you'd have to enable the PWR/BKP domain, and clocks (AHB1 BKPSRAMEN), and simply cast a structure or pointer to the memory region (0x40024000), then access it like you would any other memory. You understand how to cast to fixed addresses in C, right? uint8_t *BKPRam = (uint8_t *)0x40024000; I don't think I'd involve the compiler with generate data for this region, but rather code the application to check it's validity, and copy in some default values. I'd use a structure to manage this space.2013-03-25 3:09 PM
''i am new to stm32f4''
Do you have experience with any other microcontrollers?
Do you have experience with programming in any other environment(s)?
2013-03-27 12:10 PM
thank u clive for ur response
i just got sram working, read and write data on srami have connected VBAT 3.3V cell, and using an LSI, but when i switch off the power that is controller running on VBAT, sram does not retain valuei am posting the main function of code that i picked from stm32eval project examplesvoid RTC_Config(void){ /* Enable the PWR clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); /* Allow access to RTC */ PWR_BackupAccessCmd(ENABLE); #if defined (RTC_CLOCK_SOURCE_LSI) /* LSI used as RTC source clock*//* The RTC Clock may varies due to LSI frequency dispersion. */ /* Enable the LSI OSC */ RCC_LSICmd(ENABLE); /* Wait till LSI is ready */ while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET) { } /* Select the RTC Clock Source */ RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI); SynchPrediv = 0xFF; AsynchPrediv = 0x7F;#elif defined (RTC_CLOCK_SOURCE_LSE) /* LSE used as RTC source clock */ /* Enable the LSE OSC */ RCC_LSEConfig(RCC_LSE_ON); /* Wait till LSE is ready */ while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) { } /* Select the RTC Clock Source */ RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); SynchPrediv = 0xFF; AsynchPrediv = 0x7F;#else #error Please select the RTC Clock source inside the main.c file#endif /* RTC_CLOCK_SOURCE_LSI */ /* Enable the RTC Clock */ RCC_RTCCLKCmd(ENABLE); /* Wait for RTC APB registers synchronisation */ RTC_WaitForSynchro(); /* Write to the first RTC Backup Data Register */ RTC_WriteBackupRegister(RTC_BKP_DR0, FIRST_DATA); /* Display the new RCC BDCR and RTC TAFCR Registers */// LCD_UsrLog (''RTC Reconfig \n'');// LCD_UsrLog (''RCC BDCR = 0x%x\n'', RCC->BDCR);// LCD_UsrLog (''RTC TAFCR = 0x%x\n'', RTC->TAFCR); /* Set the Time */ RTC_TimeStructure.RTC_Hours = 0x08; RTC_TimeStructure.RTC_Minutes = 0x00; RTC_TimeStructure.RTC_Seconds = 0x00; /* Set the Date */ RTC_DateStructure.RTC_Month = RTC_Month_March; RTC_DateStructure.RTC_Date = 0x18; RTC_DateStructure.RTC_Year = 0x11; RTC_DateStructure.RTC_WeekDay = RTC_Weekday_Friday; /* Calendar Configuration */ RTC_InitStructure.RTC_AsynchPrediv = AsynchPrediv; RTC_InitStructure.RTC_SynchPrediv = SynchPrediv; RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24; RTC_Init(&RTC_InitStructure); /* Set Current Time and Date */ RTC_SetTime(RTC_Format_BCD, &RTC_TimeStructure); RTC_SetDate(RTC_Format_BCD, &RTC_DateStructure); /* Configure the RTC Wakeup Clock source and Counter (Wakeup event each 1 second) */ RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16); RTC_SetWakeUpCounter(0x7FF); /* Enable the Wakeup Interrupt */ RTC_ITConfig(RTC_IT_WUT, ENABLE); /* Enable Wakeup Counter */ RTC_WakeUpCmd(ENABLE); /* Backup SRAM ***************************************************************/ /* Enable BKPRAM Clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE); /* Write to Backup SRAM with 32-Bit Data */ for (i = 0x0; i < 0x1000; i += 4) { *(__IO uint32_t *) (BKPSRAM_BASE + i) = i; } /* Check the written Data */// for (i = 0x0; i < 0x1000; i += 4)// {// if ((*(__IO uint32_t *) (BKPSRAM_BASE + i)) != i)// {// errorindex++;// } }whereas i can see the value of sram in memory windowsram even retain the value when i load any other code, just by enabling clockcan you please tell where the issue is? are there any configuration if we connect VBAT that i missed? Thank you2013-03-29 8:44 AM
I don't have any systems with a battery hooked up in this fashion, I typically put the system in standby to turn of the primary supply/regulator.
I think you'd want some different code paths based on whether you're cold starting, or bring a system back from a power event that doesn't require a full RTC initialization. I might take a look at this, next week, in the context of my own boards, with respect to the (NV)RAM and how it is preserved.2014-03-25 1:47 AM
Hin
Just happened to be reading about this in the Reference Manual RM00090 Docdid you switch on the Backup domain Reg:-In 5.1.2 Battery backup domain''When the backup domain is supplied by VBAT (analog switch connected to VBAT because VDD is not present), the backup SRAM is powered by a dedicated low power regulator. Thisregulator can be ON or OFF depending whether the application needs the backup SRAM function in Standby and VBAT modes or not. The power-down of this regulator is controlled by a dedicated bit, the BRE control bit of the PWR_CSR register (see Section 5.4.3: PWR power control/status register (PWR_CSR)).''just skimmed you code and couldn't see this being switched on. Cheers Brian LWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.