STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Synchronizing SPI/DMA startup

Posted on March 25, 2014 at 08:23Haven't been able to find anyone discussing this. What I need to be able to do is synchronize the start of two DMA SPI transfers. The two SPI ports are running at the same clock rate, and I need an 'atomic' start to ...

STM32 with MPU 9150 MEMS

Posted on March 21, 2014 at 14:17Hi all Anybody have experienced communicating MPU-9150(DMP) with Stm32 with I2c protocol. So that can read the accelerometer, gyroscope and magnetometer data. I need a basic of it so that I can understand

sanjib by Associate III
  • 827 Views
  • 1 replies
  • 0 kudos

ADC inputs on STM3241G-EVAL Board

Posted on March 24, 2014 at 15:52Hi... I have what appears to be a simple, yet confusing issue. I have the above mentioned eval PCB. I need access to any ADC input, but they all appear to be taken. On the eval board are 4 connectors for ''daughterbo...

STM32 - two errors in turns during programming

Posted on March 24, 2014 at 21:29I'm trying to program STM32F107VCT6 via SWD and I'm constantly getting two errors in turns (literally): Error: Connect failed, check config and cable connectionError: Flash driver function execute error, Erase: [ 0...

piotr23 by Associate
  • 855 Views
  • 0 replies
  • 0 kudos

Bluetooth Stack for STM32Fxxx

Posted on March 24, 2014 at 08:04Hello,      IS there any Open Stack of bluetooth for STM32Fxxx. I have seen the lightweight mess Stack is open source, but i didn't find any where. is any one has worked on it. Please can any one suggest me on this.A...

SPI receiver register buffer question.

Posted on March 22, 2014 at 08:23I am doing an SPI write sending out dummy data to clock in the data from my SPI flash.   // Dummy data to read status register out       SPI_SendData8(SPI1, 0x05);             // Wait until transmit buffer is empty t...

assert_param error

Posted on March 24, 2014 at 15:15Hi,I just started working with stm32f10x standard peripheral library v 3.5.0. I trying to assembling project for USART, but compiller reported me .\stm32f10x_usart.axf: Error: L6218E: Undefined symbol assert_param (r...

hospodar by Associate III
  • 2258 Views
  • 4 replies
  • 0 kudos

Strange bug with STM32F407's MAC

Posted on March 21, 2014 at 12:22I'm developing a system using STM32F407ZGT with a PHY DP83848 using RMII interface. A 50MHz oscillator was used for the RMII_REF_CLK. I ran the FreeRTOS+LWIP demo application from ST's websize and encountered a stran...

Timer interrupts are not running on time.

Posted on March 24, 2014 at 01:09Hello, I'm programing a VGA signal with the STM32 discovery board. I'm using a timer to generate sync pulses and everything seems to work fine since the image shows static in the monitor. But there are some glitches,...

joecarlhr by Associate II
  • 1466 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.