2016-12-28 10:30 PM
Hello,
I'm newbie in the Bluetooth business, I purchased theSTM32L476RG Nucleo+Nucleo BLE expensionboard (X-Nucleo-IDB05A1withSPBTLE-RF module) .
Then I installed the
IAR 7.5 workbench
,copy the X-Cube-BLE1directories including the samples code - and everything works like a charm !!!As we would like to enhance ourexisting old project (based onSTM32F101CBT6andIAR5.4 workbench) with new Bluetooth BLE capabilities,
Please advise,if the samples code from the new Bluetooth BLE project (X-Cube-BLE1) can be integrated into existing old project which use the following environment, based on
STM32F101CBT6and
IAR5.4 workbench
)?
If NO, please advise,how can we overcome this obstacle.
Thanks In Advance,
Micha Valach
#st-bluetooth Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-10-06 5:10 AM
Hi
Vilei.Antonio
Sorry I havae to come back again.....
There were some changes on my board and BT_IRQ is defined as PF6 (previously it was PE1). So I changed the following#define BNRG_SPI_EXTI_IRQn EXTI9_5_IRQn
#define BNRG_SPI_EXTI_IRQHandler EXTI9_5_IRQHandlerBut now from android device it connects but after a while it disconnect saying error : 'Peripheral Disconnected!'
I think the SPI comuncation has no problem. But somehow it is getting disconected.
2017-10-06 9:26 AM
Please try enabling the debugging option for SPI by uncommenting the ♯ define PRINT_CSV_FORMAT line in 'Middlewares\ST\STM32_BlueNRG\SimpleBlueNRG_HCI\includes\debug.h' file. After you enable this option, you will see the log of the low level SPI commands and events being exchanged between your STM32 and the BlueNRG-MS chip. For example, if you are using IAR EWARM, you can see the output messages by using the View -> Terminal I/O option from the menu while you're code is being executed by the tool via ST-Link. Assuming that the SPI communication is working properly, from that log it will be easier to understand what's going on.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.