2017-10-05 4:39 AM
Solved! Go to Solution.
2017-10-06 6:09 AM
After 3 days i found a solution (or walkabout) for future reference.
/* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) { HAL_UART_Receive_DMA(&huart1, Received, 8); //start of listeningHAL_Delay(1);
if (ramka==1){ //przekierowanie rozkazu do funkcji switch(bufor[1]){ case 4:{ stany(); break; } } } ramka=0; /* USER CODE END WHILE */
i found out that when i send every 1 second order by hand it sometimes miss one or more answers, but if i send it quicker for example 5 times a sec it works perfectly. I figured that maybe there is some problem with time of creating answer so if i put a delay just outside of interrupt it might work..
And it did
2017-10-05 4:59 AM
Wouldn't call HAL_UART_Receive_DMA() blindly in a tight loop
ramka should be a volatile variable, also you don't clear it in the loop after processing the packet
2017-10-05 5:02 AM
I would use a less EMI-prone standard, like RS485 or RS422.
Your communication is package/message based, isn't it ?
Why do you call the CRC2 function on every byte, from an interrupt context ?
I have my problems understanding polish comments, though ...
2017-10-05 5:12 AM
1. ramka is cleared in mail loop after checking packet. so i wait for order, check its crc if i should process it farther, then checking what it wants me to do and then clear.
2. crc is calculated on 15/17 of final answer. last 2/17 are crc. I calculate it before sending answer in 2 parts. i copy part1 and move it to copy part2. Should i make a function for it outside of interrupt?
2017-10-05 5:29 AM
Can you tell me how to clear buffer with this:
void
TM_USART_ClearBuffer
(
USART_TypeDef
*
USARTx
)
;
maybe if i clear it after each recieve it will be enough?
2017-10-05 9:44 AM
>>ramka is cleared in mail loop after checking packet
The placement seems to create a race condition, variable should be volatile.
Enabling of DMA also seems problematic, and prone to synchronization issues.
Try implementing with a simple USART IRQ method.
2017-10-06 1:08 AM
>>The placement seems to create a race condition, variable should be volatile
i'll try it
>>Enabling of DMA also seems problematic, and prone to synchronization issues.
with DMA i'm missing less then without it, but issue is probably something else. I'll try changing it
2017-10-06 6:09 AM
After 3 days i found a solution (or walkabout) for future reference.
/* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) { HAL_UART_Receive_DMA(&huart1, Received, 8); //start of listeningHAL_Delay(1);
if (ramka==1){ //przekierowanie rozkazu do funkcji switch(bufor[1]){ case 4:{ stany(); break; } } } ramka=0; /* USER CODE END WHILE */
i found out that when i send every 1 second order by hand it sometimes miss one or more answers, but if i send it quicker for example 5 times a sec it works perfectly. I figured that maybe there is some problem with time of creating answer so if i put a delay just outside of interrupt it might work..
And it did
2017-10-06 8:38 AM
Polling with delay is possibly a workaround for Cube/HAL code, but still a bad solution.
I would drop the Cube straitjacket alltogether and go for a clear interrupt-based solution, but it's not my project.
I stopped commenting on Cube code a while ago ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.