2025-07-30 6:49 PM
I am currently evaluating the STM32G0 series for a project that requires two USB Type-C ports.
Each port needs to support both Dual Role Port (DRP) functionality and DisplayPort Alternate Mode (DP-Alt).
Can the STM32G0 be implemented?
Solved! Go to Solution.
2025-08-04 6:54 AM
Indeed, it is the same controller available on both ports. So, they have the same features.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-01 3:32 AM
Indeed, STM32G0 is the only product using 2 USB type C ports.
You can refer to the MB1352 schematics of STM32G0C1 eval daughter board as a reference.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-03 5:55 PM
Hi Support team,
Does each UCPD port on STM32G0C1 support both DRP and DP-Alt mode independently?”
2025-08-04 6:54 AM
Indeed, it is the same controller available on both ports. So, they have the same features.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.