2008-08-13 5:21 AM
Independent Watchdog when debugger is connected
2011-05-17 3:20 AM
I'm experiencing a confusing observation. When the debugger with j-link (IAR) is connected to the development board (STM32-SK from IAR) the watchdog does not reset the board.
The only reaction of the mcu is that the bit IWDGRSTF in the register RCC_CSR changes to 1 indicating a reset due to the watchdog had occurred. But it didn't. When I look into the documentation there is also a bit DBG_IWDG_STOP in the register DBG_MCU_CR which can be used to control if the watchdog should continue to run (or not) even if the core is halted. I set this bit to 0 so the watchdog should continue to run. The only configuration I see the watchdog working is when I disconnect j-link and run the code from flash.2011-05-17 3:20 AM
Hi Peter,
I have tested the same on my SK-Board, When enabling the IWDG (Reset after 500msec for example with HSI, when counter not reloaded in a while loop): the MCU does not reset. --> This behavior is due to the RT jumper ( soldered in the bottom side of he STM32-SK board. In fact this jumper is fitted ( soldered) by default and we can not remove it easily. So the pin 3 of JTAG is connected to both pin NRST and JTRST of the chip. So when the IWDG generates a reset, it will reset also the JTAG TAP and in this case it does not work well. This problem disappears when: - Using the SWD (because this pin 3 is not used by J-Link) - The J-link is not connected. I suggest you to rework the board with a simple de-soldering tool, it is very easy. Please let me if it helps. Cheers, STOne-32.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.