2022-09-22 1:06 AM
2022-09-30 3:15 AM
Wrapping is inherent in the structure of a CIC, but as long as it does not occur "too often", it works just fine. The offset is applied after the CIC stage, it does not have a relevant influence.
2022-09-30 3:32 AM
The MDF result is stored left aligned int32_t, the lower 8bits are always empty. Hence the max amplitude is +2147483392. Note that the SCALE stage has different gains.
2022-10-05 8:42 AM
@Gwenole BROCHARD
My test code on PC looks like this:
// downsample: drop D values after integrator section, then comb
// https://www.dsprelated.com/showarticle/1337.php
// the CIC uses weight * <IC> elements
// delay lines hold one element for each <IC> element of the CIC
int32_t intDelay[weight];
int32_t combDelay[weight];
memset(intDelay, 0, sizeof(intDelay));
memset(combDelay, 0, sizeof(combDelay));
unsigned j = 0;
unsigned combCnt = 0;
double cicGain = pow(downsample, weight);
for (unsigned i = 0; i < NSIZE; i++)
{
int32_t x = in[i][0];
x <<= cicShift;
for (unsigned k = 0; k < weight; k++) {
x += intDelay[k]; // sum to element in delay line
intDelay[k] = x; // store new sum in delay line
}
// downsampler
combCnt++;
if (combCnt >= downsample) {
// comb section
combCnt = 0;
for (unsigned k = 0; k < weight; k++) {
int32_t ov = combDelay[k]; // get old value from delay line
combDelay[k] = x; // add new value to delay line
x -= ov; // substract old value from new value
}
in[j++][0] = x / cicGain / (1 << cicShift);
}
}with in is the input (and output) data,
I want to run an FFT on it, so it's a two dimensional array of doubles. I only use the real part here. NSIZE is obviously the number of elements in the array.
weight is the CIC order, downsample is the decimatio ratio, cicShift is used to simulate the limited number of bits in the MDF CIC stage. cicGain has a correspondence to the MDF SCALE stage.
2022-10-24 3:13 AM
@Gwenole BROCHARD was so kind to simulate it and could not reproduce it - using the exact same setup. Since mathematics works, this claim is wrong: There must be differences in the setup.
Possible sources are:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.