2018-03-15 10:27 PM
Hi,
I have a button of size 100* on that button i want to set image for pressed and unpressed which is also of 100* I am setting it in init dialog as
BUTTON_SetBkColor(hEnter,BUTTON_CI_UNPRESSED,GUI_BLACK);
BUTTON_SetBkColor(hEnter,BUTTON_CI_PRESSED,GUI_BLACK);
BUTTON_SetBitmap(hEnter,BUTTON_CI_UNPRESSED,&bm_entericon_3Blue);
BUTTON_SetBitmap(hEnter,BUTTON_CI_PRESSED,&bm_entericon_3Pressedimageblue);
by this image is fitting into the button size .But the same thing when i am trying with call back the image is enlarged, I am not able to understand why it is like that.
callback is implemented as:
switch (pMsg->MsgId) {
case WM_INIT_DIALOG:
hEnter = WM_GetDialogItem(pMsg->hWin, ID_PW_BUTTON_12);
WM_SetCallback(hEnter, ChangeEnterButton);
break:
}
this is my callback function
void ChangeEnterButton(WM_MESSAGE * pMsg)
{
switch (pMsg->MsgId) {
case WM_PAINT:
if(BUTTON_IsPressed(pMsg->hWin))
{
GUI_SetBkColor(GUI_BLACK);
GUI_Clear();
GUI_DrawBitmap(&bm_entericon_3Pressedimageblue,0,0);
}
else
{
GUI_SetBkColor(GUI_BLACK);
GUI_Clear();
GUI_DrawBitmap(&bm_entericon_3Blue,0,0);
}
break;
default:
BUTTON_Callback(pMsg);
break;
}
}
Please do needful help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.