2015-03-03 12:12 AM
Hi I'm working on STM32F401,
I'm trying to configure I2C2 port as an I2C Master, when i Generate START condition i don't get an interrupt.What I'm doing wrong?
//Configure PB10 I2C2 Master, SCL pin PB3 I2C2 Master SDA pin GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3|GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOB, &GPIO_InitStructure); // init GPIOB //Configure the NVIC for I2C2 MASTER NVIC_InitStructure.NVIC_IRQChannel = I2C2_EV_IRQn;// Configure the I2C event priority NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 6; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 6; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = I2C2_ER_IRQn;// Configure I2C error interrupt to have the higher priority NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 7; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 7; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_SetPriority(I2C2_EV_IRQn ,6 );//I2C2 MASTER NVIC_SetPriority(I2C2_ER_IRQn ,7 );//I2C2 MASTER I2C_InitTypeDef I2C_InitStruct; I2C_DeInit(I2C2); // enable APB1 peripheral clock for I2C2 RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);/*SCL GPIO clock enable */ RCC_APB1PeriphResetCmd(RCC_APB1Periph_I2C2, ENABLE);/* Reset I2Cx IP */ // Connect I2C2 pins to AF GPIO_PinAFConfig(GPIOB, GPIO_PinSource3, GPIO_AF9_I2C2); // SCL GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_I2C2); // SDA // configure I2C2 I2C_InitStruct.I2C_ClockSpeed = 400000; // 400kHz I2C_InitStruct.I2C_Mode = I2C_Mode_I2C; // I2C mode I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2; // 50% duty cycle --> standard I2C_InitStruct.I2C_OwnAddress1 = 0x00; // own address, not relevant in master mode I2C_InitStruct.I2C_Ack = I2C_Ack_Disable; // disable acknowledge when reading (can be changed later on) I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; // set address length to 7 bit addresses I2C_Init(I2C2, &I2C_InitStruct); // init I2C3 // enable I2C2 I2C_Cmd(I2C2, ENABLE); I2C_ITConfig(I2C2, (I2C_IT_EVT | I2C_IT_BUF), ENABLE);// Enable Event Interrupts I2C_AcknowledgeConfig(I2C2, ENABLE);// Enable Acknowledge I2C_GenerateSTART(I2C2, ENABLE);// Generate the Start condition2015-03-03 4:11 AM
This needs to be enabled BEFORE GPIO_Init()
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
2015-03-03 4:38 AM
Thanks,
I did this & it's steel doesn't works, I get on SR2 register BUSY=1. Both lines SDA and SCL are HIGH.2015-03-03 4:59 AM
// enable I2C2
I2C_Cmd(I2C2, ENABLE);
// configure I2C2
I2C_InitStruct.I2C_ClockSpeed = 400000; // 400kHz
I2C_InitStruct.I2C_Mode = I2C_Mode_I2C; // I2C mode
I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2; // 50% duty cycle --> standard
I2C_InitStruct.I2C_OwnAddress1 = 0x00; // own address, not relevant in master mode
I2C_InitStruct.I2C_Ack = I2C_Ack_Disable; // disable acknowledge when reading (can be changed later on)
I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; // set address length to 7 bit addresses
I2C_Init(I2C2, &I2C_InitStruct); // init I2C2
2015-03-03 5:36 AM
Thanks,
I did this & it's steel doesn't works, I get on SR2 register BUSY=1. Both lines SDA and SCL are HIGH.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.