2014-07-21 12:43 AM
Hi everyone I am Khai.
Currently I am working with STM32F103ZE. I would like to test on clock stretching by using a delay()-function. But seems like it doesn't work. Any advice or suggestion on how to make a test for clock stretching? Belows are my written code:INIT
void I2C_Initi (I2C_TypeDef *i2cx, int OwnAddress, I2C_Callback_t *callWr, I2C_Callback_t *callRd) { I2C_InitTypeDef I2C_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; uint32_t clock_en; callbackWr = callWr; callbackRd = callRd; switch((unsigned int)i2cx) { case (unsigned int)I2C1: clock_en = RCC_APB1Periph_I2C1; break; case (unsigned int)I2C2: clock_en = RCC_APB1Periph_I2C2; break; default: printf(''I2C_Initi bad i2cx %p'',i2cx ); return; break; } RCC_APB1PeriphClockCmd(clock_en, ENABLE); I2C_StructInit(&I2C_InitStructure); I2C_InitStructure.I2C_ClockSpeed = 100000; I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = OwnAddress; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_Init(i2cx, &I2C_InitStructure); I2C_ITConfig(i2cx, I2C_IT_BUF|I2C_IT_EVT|I2C_IT_ERR, ENABLE); I2C_Cmd(i2cx, ENABLE); I2C_StretchClockCmd(i2cx, ENABLE); // configure NVIC I2C interrupt NVIC_InitStructure.NVIC_IRQChannel = I2C2_EV_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x01; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = I2C2_ER_IRQn; NVIC_Init(&NVIC_InitStructure); }INTERRUPT HANDLER
void I2C2_EV_IRQHandler(void) { uint32_t event; //I2C_StretchClockCmd(I2C2, ENABLE); //delay_us(I2C_Delay); event = I2C_GetLastEvent(I2C2); switch(event) { // sending to MASTER case I2C_EVENT_SLAVE_TRANSMITTER_ADDRESS_MATCHED: I2C_SendData(I2C2, i2c_buf_tx[0]); tx_count=1; break; case I2C_EVENT_SLAVE_BYTE_TRANSMITTED: I2C_SendData(I2C2, i2c_buf_tx[tx_count]); tx_count++; if(tx_count>=i2c_send_len-1) GPIO_S(gpios+GPO_HOOK_PTT, 0); break; case I2C_EVENT_SLAVE_ACK_FAILURE: /// tell main loop it is done, for example setting i2c_send_len to 0 if(callbackRd) callbackRd(tx_count, (uint8_t*)i2c_buf_tx); tx_count=0; break; // receiving from MASTER case I2C_EVENT_SLAVE_RECEIVER_ADDRESS_MATCHED: I2C_StretchClockCmd(I2C2, ENABLE); delay_us(I2C_Delay) ; // delay 20 us //i2c_buf_rx[0]=I2C_ReceiveData(I2C2); //rx_count=1; break; case I2C_EVENT_SLAVE_BYTE_RECEIVED: delay_us(I2C_Delay); // delay 20 us //I2C_StretchClockCmd(I2C2, ENABLE); i2c_buf_rx[rx_count]=I2C_ReceiveData(I2C2); rx_count++; break; case I2C_EVENT_SLAVE_STOP_DETECTED: delay_us(I2C_Delay); // delay 20 us //I2C_StretchClockCmd(I2C2, ENABLE); if(callbackWr) callbackWr(rx_count, (uint8_t*)i2c_buf_rx); I2C_AcknowledgeConfig(I2C2, ENABLE); rx_count=0; break; default: err_count++; err_event = event; break; } last_event = event; } Thank you. #i2c-stm32We’re moving the ST Community to a new platform to give you a better and more reliable community experience.