2018-08-16 4:26 PM
Hi,
I am working on I2C read EEPROM. The HAL function failed due to the I2C_FLAG_BUSY is always SET.
Is there anything I am missing in init code?
Thx
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY, tickstart) != HAL_OK)
{
return HAL_TIMEOUT;
}
2018-08-16 5:23 PM
this code works:
note the address is shifted up 1 bit...
#define MCP4728_DacAddress 0x60 << 1
void write4Dacs(void) {
char buf[16];
struct DacIIC MCP4728IIC;
HAL_StatusTypeDef IIC_Response;
// Dac_Value = (4096 * 1) / 5; // 1V
//Channel 0
MCP4728IIC.DacTxBuffer[0] = (Dac0_Value & 0x0f00) >> 8;
MCP4728IIC.DacTxBuffer[1] = Dac0_Value & 0x00ff;
//Channel 1
Dac1_Value = Dac0_Value + (4096 * 1) / 5; // 1V
MCP4728IIC.DacTxBuffer[2] = (Dac1_Value & 0x0f00) >> 8;
MCP4728IIC.DacTxBuffer[3] = Dac1_Value & 0x00ff;
//Channel 2
Dac2_Value = Dac1_Value + (4096 * 1) / 5; // 2V
MCP4728IIC.DacTxBuffer[4] = (Dac2_Value & 0x0f00) >> 8;
MCP4728IIC.DacTxBuffer[5] = Dac2_Value & 0x00ff;
//Channel 3
Dac3_Value = Dac2_Value + (4096 * 1) / 5; // 3V
MCP4728IIC.DacTxBuffer[6] = (Dac3_Value & 0x0f00) >> 8;
MCP4728IIC.DacTxBuffer[7] = Dac3_Value & 0x00ff;
//DAC_IIC.write(DAC_ADDR + (Dac_Address << 1), buf, 8);
IIC_Response = HAL_I2C_Master_Transmit(&hi2c1, MCP4728_DacAddress, &MCP4728IIC.DacTxBuffer[0], 8, 10);
}
2018-08-17 9:25 AM
The issue is I2C_FLAG_BUSY is always SET. That's why this function bailed out after timeout.
We are using 24AA02E48 to get EUI-48. Thx
static HAL_StatusTypeDef I2C_WaitOnFlagUntilTimeout(I2C_HandleTypeDef *hi2c, uint32_t Flag, FlagStatus Status, uint32_t Timeout, uint32_t Tickstart)
{
while (__HAL_I2C_GET_FLAG(hi2c, Flag) == Status)
2018-08-17 9:39 AM
I checked the I2C registers. ISR register value is 0x8009 (1000000000001001) which means bit 15 is set in HAL_I2C_Mem_Read() function.
I also check the flag before call read. Not sure how to turn it off.
uint32_t flag = __HAL_I2C_GET_FLAG(m_i2c, I2C_FLAG_BUSY);
Bit 15 BUSY: Bus busy
This flag indicates that a communication is in progress on the bus. It is set by hardware when a
START condition is detected. It is cleared by hardware when a STOP condition is detected, or
when PE=0.
2018-08-17 3:23 PM
Sorry to catchup, which part ?
what address are you using ?
on initisation the errent flag is set or not ?
try power off and then check the flag it should be clear.
then check the DAC code I sent... I don't check any flags, it just works.
which part ? and what address is it ?
and show us the first line of transmit.
2018-08-17 4:02 PM
I am using STM32L4A6VG MCU connecting I2C 2 to Microchip 24AA02E48 EEPROM (2K I2C Serial EEPROMs with EUI-48™ or EUI-64™ Node Identity) for EUI-48 ID.
http://ww1.microchip.com/downloads/en/DeviceDoc/20002124G.pdf
There is no transition happened at all since all of checking before TX/RX. I am able to DISABLE/ENABLE I2C to make the first BUSY flag go away. Now I am seeing this TXIS flag is not set. Thx
/* Wait until TXIS flag is set */
if (I2C_WaitOnTXISFlagUntilTimeout(hi2c, Timeout, Tickstart) != HAL_OK)
2018-08-17 4:11 PM
how are the pins A0 A1 A2 set ? 0,0,0 ?
thats 0xA0 for Write and 0xA1 for Read,
are you using just one device on the IIC bus ?
in my code there is no initialisation, it just works...
2018-08-17 4:23 PM
Thanks for the input. Just figured out the way our layers of driver works should OR 0x01 before calling 24AA02E48 driver. Thanks a lot.
m_i2c->read_from_address(0b10100000, 0xFA, 1, in_data, in_len);
2018-08-17 4:38 PM
I still have the same error with the READ address modified. Thx
2018-08-17 4:41 PM
I guess you are using blocking code, and you are read/nested read/nested read/stopped/// I guess
can you try this ?
POWER OFF for 5 seconds
READ ONCE only.
wait 1 second
READ again
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.