2017-05-16 2:14 PM
Hello friends
I want to using the functions HAL To connect with AT24C64
To Byte Write & Byte Read How can I send data as below:
I've searched but did not find the answer
Thank
#i2c-eeprom-example-hal2017-05-17 3:39 AM
instead of using address 0xA0 use the address (uint16_t)(0x50<<1) as the HAL wants the address left aligned
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.