2019-01-03 2:53 AM
All ADCs are in regular mode and only 1 channel is used per ADC.
I can get ADCs 1,2 and 3 to work, but when ADC 4 is added it never generates an interupt.
If I only start ADCs 3 and 4 it works fine.
Everything is generated with CubeMX (find attached file-Test_adc).
The main file is also uploaded (main)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.