2023-02-23 12:58 AM
In my project, I convert char array components to uint_8 data type with atoi. It works fine with my project in the debug phase, then it doesn't work. I have to debug every time I want to run it.
/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if(huart->Instance==USART1)
{
// if the character received is other than 'enter' ascii13, save the data in buffer
if(rx_data!=13)//
{
buffer[rx_index++]=rx_data;
}
else
{
// if new message arrived, read the message
if(sscanf((char*)buffer, "\n+CMTI: " PREF_SMS_STORAGE ",%hhd", &slot)==1)
{
sprintf(ATcommand,"AT+CMGR=%d\r\n",slot);
HAL_UART_Transmit_IT(&huart1,(uint8_t *)ATcommand,strlen(ATcommand));
}
// if message read contains "ledon", switch the LED ON
else if (strstr((char *)buffer,"ledon"))
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_13, 1);
sprintf(msj,"Led acildi");
msjDrm=1;
}
// if message read contains "ledoff", switch the LED OFF
else if (strstr((char *)buffer,"ledoff"))
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_13, 0);
sprintf(msj,"Led kapandi");
msjDrm=1;
}
// This will delete all messages in the SIM card. (Is it ok for you?)
else if (strstr((char *)buffer,"READ"))
{
sprintf(ATcommand,"AT+CMGD=,4\r\n");
HAL_UART_Transmit_IT(&huart1,(uint8_t *)ATcommand,strlen(ATcommand));
}
else
{
/************* ayarlamLAR *************/
char destination[25];
int start = 1;
int len = 2;
substring(destination, (char *)buffer, start, len);
if (strstr((char *)destination,"ch"))
{
/***********kanal************/
veri[0]=buffer[3];
veri[1]=buffer[4];
kanal = (uint8_t)atoi(veri);
/***********adres************/
veri[0]=buffer[5];
veri[1]=buffer[6];
adres = (uint8_t)atoi(veri);
/*****hangı cıkıs?******/
veri[0]=buffer[7];
veri[1]=buffer[8];
cikis_ = (uint8_t)atoi(veri);
if (cikis_== 1)
{
veri[0]=buffer[9];
veri[1]=buffer[10];
drm = (uint8_t)atoi(veri);
veri[0]=buffer[11];
veri[1]=buffer[12];
baslangic_h = (uint8_t)atoi(veri);
veri[0]=buffer[13];
veri[1]=buffer[14];
baslangic_m = (uint8_t)atoi(veri);
veri[0]=buffer[15];
veri[1]=buffer[16];
bitis_h = (uint8_t)atoi(veri);
veri[0]=buffer[17];
veri[1]=buffer[18];
bitis_m = (uint8_t)atoi(veri);
}
Tx_data[0]=0x00;//başlangıc biti
Tx_data[1]=adres;//adress
Tx_data[2]=kanal;// kanal
Tx_data[3]=drm;//0
Tx_data[4]=baslangic_h;
Tx_data[5]=baslangic_m;
Tx_data[6]=bitis_h;
Tx_data[7]=bitis_m;//0
Tx_data[8]=8;
Tx_data[9]=9;
Tx_data[10]=9;
Tx_data[11]=9;//0
Tx_data[12]=9;
Tx_data[13]=9;
Tx_data[14]=9;
Tx_data[15]=8;//0
Tx_data[16]=8;
Tx_data[17]=8;
Tx_data[18]=8;
Tx_data[19]=7;//0
Tx_data[20]=7;
Tx_data[21]=7;
Tx_data[22]=7;
Tx_data[23]=7;//0
Tx_data[24]=7;
Tx_data[25]=7;
Tx_data[26]=7;
Tx_data[27]=7;//0
Tx_data[28]=7;
Tx_data[29]=7;
Tx_data[30]=7;
Tx_data[31]=7;//0
Tx_data[32]=7;
Tx_data[33]=7;
// HAL_UART_Transmit(&huart3, Tx_data, sizeof(Tx_data), 100);
sprintf(msj,"YAZDIRILDI");
msjDrm=1;
}
}
rx_index=0;
memset(buffer,0,sizeof(buffer));
}
}
// Enabling interrupt receive again
HAL_UART_Receive_IT(&huart1,&rx_data,1); // receive data (one character only)
}
/* USER CODE END 4 */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.