2022-12-23 12:06 AM
Should I give up on the STM32H series and move to the STM32MP series?
2022-12-23 1:17 AM
>>Is this a push to shift technologies?
chips everyone is using have been 2 years drying out, chips that noone is using (because they are too new) are available.
St is not even able to steadily provide STLinks, i would blame the thisone to postcovid market
Since last year i always develop multifootprint pcb layouts to be able to shift from one mcu to another without disrupting the production line too much.
Normally i do TFBGA inside a LQFP if the mcus need a bit of rerouting, but normally just stay with LQFP and a couple of 0R jumpers (the reflow oven hates BGA).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.