2017-12-11 2:59 AM
hello.
i used STM32F103 MCU, and hope to stop mode with wake-up by EXTI.
By googling, i could operating stop mode and wake-up. BUT...
i confirmed that STM32 dissipated over 40mA at stop mode, without any other hardware.
when i disabled PC6 GPIO, i saw a reducing current.
let me know what i have to check the source or hardware.
i don't know what is problem. plz help me.
void main(void)
{
SystemInit(); // Setup STM32 System
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE); // power interface clock, backup interface clock
Interface_Init(); // Interface Initialize
EXTI0_Config();
while (1)
{
PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI);
}
}
void EXTI0_IRQHandler(void)
{
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
{
/* do something */
SYSCLKConfig_STOP_Run();
GPIO_WriteBit(GPIOC, GPIO_Pin_6, Bit_SET);
updatePacket();
GPIO_WriteBit(GPIOC, GPIO_Pin_6, Bit_RESET);
/* Clear the EXTI line 0 pending bit */
EXTI_ClearITPendingBit(EXTI_Line0);
}
}
void Interface_Init (void)
{
NVIC_InitTypeDef NVIC_InitStructure;
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOC, ENABLE);
RCC_ADCCLKConfig(RCC_PCLK2_Div6); //clock for ADC (max 14MHz, 72/6=12MHz)
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); //enable ADC clock
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
/* Configure PC output */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 ;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;//GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Configure UART Tx */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Configure UART Rx */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOA, &GPIO_InitStructure);
NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
}
2017-12-12 9:26 AM
You must care for each GPIO. GPIO may only float when configureds as 'analog'. Otherwise provide Pull UP or down.
2017-12-12 9:58 AM
>>without any other hardware
So what's PC6 connected too? And how about PA9/PA10?
2017-12-12 3:19 PM
PC6 is used as GPIO, and PA9/PA10 are USART ports.
Any other GPIO ports was set to Analog-in.
I doubt that I was wrong about code of EXTI0_IRQHandler.
How about your thought.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.