2009-02-09 1:27 AM
I can not use SDIO in 4bit Bus DMA mode
2011-05-17 4:00 AM
I tested STM32 SDIO for several days and
found the following appearance: 1. while (1) { SD_ReadBlock(); SD_ReadBlock(); } Test Passed 2. while (1) { SD_ReadMultiBlocks(); SD_ReadMultiBlocks(); } Test Passed 3. while (1) { SD_WriteBlock(); SD_ReadMultiBlocks(); } Test Error: SD_START_BIT_ERR 4. while (1) { SD_WriteBlock(); Delay_ms(1000); SD_ReadMultiBlocks(); } Test Ok: SD Card : KingSton 2G. SDIO Mode: DMA+4bitsBus I have read the relaxe's code ''SDIO_DosFS_V02.zip''. but not found any SD_ReadMultiBlocks/SD_WriteMultiBlocks in it. who can give me some helps about SD_ReadMultiBlocks/SD_WriteMultiBlocks Operation in 4bitBus+DMA mode ? Thanks a lot.2011-05-17 4:00 AM
Hi there!
Nope, my SDIO_DosFS_V02.zip does not have multi-block read/write, only multiple single blocks, as the DosFS library does not discriminate 1 or multi block in line. I am however working on a third version that may include that, as I need more speed for my projects. The Read/Write (single) code actually start a DMA transfer, then wait for the TX/RX_Empty flag from the DMA, in a blocking function. Maybe the read/write multi actually works in a similar way, but without the last ''wait''? Instead of a delay, if you looked at the DMA empty flags? -RelaxeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.