2009-02-09 1:27 AM
I can not use SDIO in 4bit Bus DMA mode
2011-05-17 3:59 AM
my test environment:
STM3210E, 4G SD card , SDIO 4bits bus, DMA mode The Results are : 1. R/W 512M SD card is ok. 2. R/W 4G SD card is deadlock, at while (DMA_GetFlagStatus(DMA2_FLAG_TC4) == RESET); 3. Change Bus to 1bit , R/W 4G SD card is Ok any one have passed R/W SDHC card by SDIO in DMA 4bits mode ?2011-05-17 3:59 AM
Don't have an exact answer/guidance - sorry.
Believe that any SD card - 4GB & up - uses SD-HC. The HC requires a slightly different treatment. Seem to recall that STOne-32 posted a solution enabling SD-HC within the past 60 days. Good luck...2011-05-17 3:59 AM
What version of the library do you use?
Are you using the plain example from the SDIO folder? I currently play around with various SD and SDHC from 15mb to 4GB and everything works great..... Are you using the dev board, or do you have a voltage-translating buffer? Have you tried to apply power to the card (and wait), then remove-re-insert the card, then execute code? Solved some weird card initiation bugs...2011-05-17 3:59 AM
@relaxe-
Good info (as usual) - thank you. Would you be so good as to tell us make/model of 4GB which worked? (we've found some brands ''buggy'' - could be us, though) Thanks...2011-05-17 3:59 AM
Yeah sure!
From lower to higher capacity: MicroSD 128MB, unknow brand came with STM3210E-EVAL: SMS128FFE5 SD 2GB Kingston: MMAGF02GWWCA-NA , FB4L0000 804 MicroSDHC 4GB Sandisk: No numbers, came in a bundle with a SD adapter SDHC 4GB Ultra: G04GNM26B0040 SDHC 16GB Patriot: PSF16GSDHC6-PC .. I =THINK= (not sure) that I managed to get a A-Data/MyFlash SD 4GB working too. I know there are provision for those non-sdhc 4gb cards in the SDIO application exemple but I need 16GB and more anyway, so I don't bother. -Relaxe2011-05-17 3:59 AM
@relaxe-
Great - thank you. Lowest cost Micro SD 2GB we've found is PNY 11.88 USD Q 1. Trying to make quantity purchase for this forum - (like pulling teeth - glad some firm has money - PNY shows little interest in sales)2011-05-17 3:59 AM
hi relaxe,
Test environment: Hardware: EK-STM3210E MicroSD 4G Kinstone Mark:0850 K87866Y Test Code: um0427_Firmware library\FWLib\examples\SDIO sdcard.c V2.0.3 09/22/2008 MCD Application Team library: * File Name : stm32f10x_sdio.c * Author : MCD Application Team * Version : V2.0.3 * Date : 09/22/2008 Power: By USB Port Of PC; 1. I can read or write 4G SD card with 1bits bus mode. it means power is ok. 2. I use PC to read/Write this 4G SD card ,no any problem. 3. Can you run your test code with 4bits bus mode or 4bits bus+DMA mode? 4. would you show me your test code ? Thanks2011-05-17 3:59 AM
My guess is that you have a 4GB ''SD'' card, and not a 4GB ''SDHC'' card.
I don't want to sound like a dick, but: Ditch the card, and get a new SDHC one. 4GB SD card are not ''SD Compliant'' by nature. Do you have the same problems with other cards? Is it a ''SDIO port'' problem, or ''Some specific card'' problem? What I used to read/write to SDcards is the same exact code than you. If you are able to just open the project file, and run it on the board, then you do the same exact thing as me.2011-05-17 4:00 AM
Any SD card which is big than 2G is 'SDHC'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.