2025-09-28 10:51 AM
Hello,
I am trying to get f_mount() to work with the SDIO peripheral.
Currently, the f_mount() reaches the first disk_read() function, where it hangs in the osMessageQueueGet() call.
Stuff I already tried:
- increase min & max heap to 0x400, 0x800
- increase default static rtos task stack size to 8000
- call f_mount in the default task
- have delay before f_mount
- pullup on all IO pins except the CLK
- the hsd.Instance has recognized card type and class
- the NVIC prio is 5 for SDIO and DMA stream
- tried SDIO_RX/SDIO_TX combo and just SDIO
- tried setting GPIO pins to lower speeds
- tried SD bit 1 mode and then switching to 4bit mode
- tried SD bit 1 mode and keeping 1 bit mode
- SDIO_IRQ interrupt hits, but does not put anything in the SDQueueID queue.
i would prefer to use the cubemx generated drivers and not write one myself. is this configuration (RTOS+SDIO+FATFS) not possible/bugged?
thanks.
2025-09-29 3:20 AM
Hello @ayhamxyz
Please refer to the example below as starting point.
@ayhamxyz wrote:- the NVIC prio is 5 for SDIO and DMA stream
The interrupt priority is too high (must be lower than the RTOS kernel interrupt priority which is 5).
2025-09-29 10:23 PM
I tried that with no avail,
I am using the automatically generated SDIO dma template driver from stm32cubemx/ide, which follows closely the project @Saket_Om linked, except that I am using CMSISv2, so it is using the newer osQueue* functions.
I tried to use f_mount() with a new project, no rtos, no dma, and that did not work. I used 2 different SDcards, both are SanDisk, one is a newer 128gb and another is 32gb (older HD version). The SDIOCLK divisor is 4, so that should work.
I am starting to suspect that it is a PCB issue.
Thanks for your reply anyhow.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.