2018-10-28 4:49 AM
with the help of the HAL code library i am able to see the output while using LOOPBACK mode in CAN but at the same time not able to get the data in the NORMAL mode . can any one help me out with this problem ?
thanks in advanced
2018-10-29 3:20 AM
The NUCLEO board doesn't ship with CAN transceivers you'll need to port code from an EVAL board that does. I could probably port the code but it would take time and money. You need two nodes with compatible settings for the bus to function.
The loop back mode self acknowledges, in normal mode another node needs to do that, and needs the same rate settings.
2018-10-29 3:28 AM
Thank you i am having CAN transceivers and both the node are having same configurations you kindly refer my code i have attached .
2018-10-29 3:47 AM
Can you and your colleague work together perhaps and not carry two threads on materially the same topic?
2018-10-29 3:55 AM
yes we are working together only but at the same we don't know who will give answer to thread and whose not right ? so may some other person can answer the thread which he asked so we thats the reason to post the thread and finally our hope to get help from the STcommunity person and resolve the issue which we are facing . so please can you help out for this ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.