2021-03-17 5:18 PM
2021-03-17 5:26 PM
Which USB are you connecting too?
You're going to have to be responsible for fixing the USB Device code you've written and loaded onto the STM32 in question.
2021-03-17 5:31 PM
I am using both USB ports on the Nucleo board. This board is an EVB given to me by a chipset vendor who is using the Nucleo board to control their chip. I do not have access to the source code but want to test the chip as I have in the past.
2021-03-17 9:49 PM
You'll need to work with that vendor to get their software working, or get a new copy of the software if you have erased the load that was on the board.
Broadcom?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.