2021-07-02 9:23 AM
I am using STM32H753ZI Nuccleo board. When I configure it on cube, I am using independent mode (otherwise no ADC works).
I was only able to make them work together by stopping the running ADC in the conversion completion interrupt and raise a flag to start the other one. The problem is that I need both of them to run together without enabling and stopping the ADC_DMAs.
Solved! Go to Solution.
2021-07-02 11:22 AM
You didn't answer the middle question, but if OVR is set, you're likely converting too fast.
2021-07-02 10:00 AM
Examine registers when they don't work. Do any overflow flags get set? How fast are the conversions? What does the one "not working" mean exactly?
2021-07-02 11:09 AM
..
2021-07-02 11:21 AM
@TDK The one not working means there is no values read from the ADC. The ADC that works is the first one initialized. and yes, I have an OVR in the ISR register.
2021-07-02 11:22 AM
You didn't answer the middle question, but if OVR is set, you're likely converting too fast.
2021-07-02 11:32 AM
I could use some help answering the middle question..
2021-07-02 11:32 AM
I am having the 2 ADCs with the same settings, except for the GPIO pins and the DMA1Stream0/1
2021-07-02 11:35 AM
> I could use some help answering the middle question..
If ADCs are freerunning, as opposed to being triggered off of a timer, they are running as fast as possible. Since the bus is a shared resource, this can overwhelm the bus. If a new conversion is done before the DMA ships off the last value, the ADC will report an overrun and stop.
You can decrease the conversion rate by increasing the sample time under channel configuration settings, or setting it up to run off of a timer TRGO output.
Including relevant code along with your post, or an IOC file, can help explain what you're doing.
2021-07-02 11:45 AM
OK, so I made the prescaler divided by 4, and it is working now. Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.