2025-05-05 11:53 AM
Hi
I have a VERY large driver for a PSFB that unfortunately suffer from a flaw.
The idea is that the master timer is reporgrammed with period and CMP1 CMP2 and CMP3 and that the timerD and timerE uses these 4 points for the crossbar. Everything works correctly except for how the new values are taken into account.
The timers have preload enabled so, I expected that I could use LL_HRTIM_SuspendUpdate and LL_HRTIM_ResumeUpdate after i have changed the prescaler, period and Compare 1,2 and 3. But that does nothing. I need to actually use LL_HRTIM_ForceUpdate which obviously sometimes will then break my waveform as the transfer from the shaowregisters are not done during an rollover.
Does someone have a working example of LL_HRTIM_SuspendUpdate/LL_HRTIM_ResumeUpdate that they are willing to share or does someone know why this behaviour occur?
I am using stm32G474 and HAL/LL 1.6.1
Best regards
Martin
2025-05-06 12:49 AM
For anyone who get the same symptoms:
Setting LL_HRTIM_TIM_SetUpdateTrig to LL_HRTIM_UPDATETRIG_NONE will get you these symptoms, which is pretty obvious. Changeing it to LL_HRTIM_UPDATETRIG_REPETITION or LL_HRTIM_UPDATETRIG_RESET will get the desired behaviour
// Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.