2018-08-02 1:30 AM
Hi everbody. From the <<PM0075 Programming manual>> ,I have success erase the entire flash follow Mass Erase sequence, the C code as below:
FLASH_Status flashEraseAllOptionBytes_STM32(void)
{
FLASH_Status status = FLASH_COMPLETE;
uint32_t flash_CR,flash_SR;
flash_CR = readMem((uint32_t)&(FLASH->CR));
flash_CR |= CR_MER_Set;
writeMem((uint32_t)&(FLASH->CR), flash_CR);
flash_CR |= CR_STRT_Set;
writeMem((uint32_t)&(FLASH->CR), flash_CR);
status = FLASH_WaitForLastOperation(((uint32_t)0x000B0000));
return 0x09;
}
But I don't know how to do write the flash by SWD?
2018-08-02 5:43 AM
SWD based programmers typically download a small applet to RAM which implements the FLASH Erase/Write functionality, taking data buffered in RAM and updating the FLASH.
Your tools would therefore need to be able to download the app/data to RAM, and then execute that code. Process repeats until you fully program device. I wouldn't try to drive the FLASH peripheral via the SWD directly.
2018-08-02 7:19 AM
Thank you for your help . I don't konw how the kind of writeing app to ARM . So first , I want to write the Flash directly by SWD for Prove that my code will be ok, and second write app to ARM。 Mabe your have the code of writeing app to ARM?
2018-08-02 7:54 AM
Maybe I do.
You should perhaps start by looking at the FLASH examples for the specific STM32 part(s) you are targeting, and build and test those.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.